Calibration Instrumentation Specifications
When you calibrate the analog input modules, send current reference signal to the
module to calibrate it. To maintain your module's factory calibration accuracy, use
the instrumentation with the specifications listed in the following table.
IMPORTANT:
Do not calibrate your module with an
instrument that is less accurate than those specified in following table. The
following events can result:
- Calibration appears to occur normally but the module gives inaccurate data during operation.
- A calibration fault occurs, forcing you to abort calibration. When this happens, I.Chxx.CalFault tag is set for the channel you attempted to calibrate. You can clear this tag by completing a valid calibration or cycling power to the module.
Catalog Number | Channel Input Type | Calibration Instrumentation Specifications |
|---|---|---|
5034-IF8C and 5034-IF8CXT | Current (mA) | 4.00…20.00 mA source ±100 nA current |
Provide Feedback