Syslog Routing Settings
Below are settings for enabling and configuring Syslog in
FactoryTalk® Policy Manager
.Syslog routing
Property | Description |
|---|---|
Enable syslog routing using syslog server | Enables devices that support syslog routing to start sending Syslog messages as configured in the policy. These settings apply to all devices that support syslog routing. |
Property | Description |
|---|---|
IP Address | Identifies the Syslog server by the IP address. |
Hostname | Identifies the Syslog server by the DNS host name. |
Port | Identifies the communications port on the server to receive the Syslog messages. Default port number is 514. |
Protocol | Configures logging.
|
Property | Description |
|---|---|
Event types that will generate messages | Used to determine which event types generate messages.
|
Lowest level of severity to log | Logs messages that are greater than or equal to the severity level selected. Defined severity levels from highest to lowest are:
|
Property | Description |
|---|---|
Details to include in message | Specifies details included in the message.
|
Time resolutions | Defines the level of precision used in the time stamp of the log messages:
|
Provide Feedback