Vendor Sample Projects command

Choose this command to launch the
Vendor Sample Projects .pdf
file to access sample projects from Rockwell Automation and several other vendors. Use these sample projects with products from those companies. Refer to the PDF file for more information.
Important:
Some browsers (particularly the Edge browser) will not launch the
Logix Designer
application from the ACD hyperlinks in the PDF file when configured to open PDF files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal