Message Configuration Dialog Box - Status Section Overview

This area of the
Message Configuration
dialog box lets you see and manipulate the part of the message tag available from the Data Monitor.
Parameters
Enable
This field lights up blue when the Enable bit is true. This bit signifies that user logic has attempted to trigger the message.
Enable Waiting
This field lights up blue when the Enable Waiting bit is true. This bit signifies that the message has been triggered, but processing of the configured request has not yet begun.
Start
This field lights up blue when the Start bit is true. This bit signifies that the message processing has begun.
Done
This field lights up blue when the Done bit is true. This bit signifies that the message processing was successfully performed to completion.
Done Length
Displays the amount of data actually transferred (0...65335). This may be in elements or in UNITs, depending on the service code.
Error
This field lights up blue when the Error bit is true. This bit signifies that that message processing resulted in an error. You must select
Error Code
to view the error.
Error Code
The Hex value (UINT) of the message error code (0 to 0xFFFF).
Timed Out
Displays and lets you select the value of the Timed Out requested bit. This bit signifies that you have requested that message processing be terminated. You select this bit to time out the message instruction. Once you select this item, the value is immediately updated, as indicated by the blue arrow to the right of it.
Extended Error Code
The Hex value (UINT) of the message extended error code (0 to 0xFFFF). This value is only valid if the message extended error code length is 1. If the extended error length is 0, no extended error code is available. If the extended error length is greater than 1, then the error information is placed within the destination tag. You must then go to the Data Monitor to view this information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal