HMIBC Properties dialog box - Status tab

The
Status
tab displays the current status of every HMI device that is currently interacting with the HMIBC tag.
Parameters
HMIBC Devices
The following information is displayed:
  • HMI Device's Name
  • HMI Device's IP Address
  • HMI Device State
Each HMI device that is interacting with an HMIBC instruction can be in one of three states:
  • Idle - A button that is associated with the HMIBC tag on this HMI device is not currently being pressed. The HMI device has a valid connection to the controller.
  • Triggered - A button that is associated with the HMIBC tag on this HMI device is being pressed. The HMI device has a valid connection to the controller.
  • Connection Faulted - The HMI device does not have a valid connection to the controller. (The button state is unknown.)
The information on the
Status
tab is read-only.
The list of HMI devices, including the state of the buttons, is updated every few seconds.
If there are no HMI devices registered with the HMIBC tag, then <None> displays.
If the controller is offline, then <Offline> displays.
Execution Order Number (Function Block Diagram routine only)
Displays a number that identifies the execution order of the instruction.
Never display description in a routine (Function Block Diagram routine only)
Select if you do not want the description to display in the routine.
This option is not selected by default.
OK
Click this button to accept your edits and to close the HMIBC Properties Status dialog box.
Cancel
Click this button to close the
HMIBC Properties
dialog box without applying your edits.
Apply
Click this button to apply your edits and continue editing in the
HMIBC Properties
dialog box.
Help
Click this button for help on the
HMIBC Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal