Generate Signature Report command

Choose this command to generate a safety signature report that shows when each safety element last changed. The most recent changes are highlighted in a style similar to the Compare Tool.
The generated safety signature report is displayed in a Web browser. A copy of the safety signature report is also saved in this folder:
C:\\Users\Public\Documents\Rockwell Automation\Studio 5000\Logix Designer\Safety Signature Reports
The file name of the saved safety signature report is comprised of the project name and current date and time.
For a complete overview of safety signature elements, see the ControlLogix 5580 and GuardLogix 5580 Controllers User Manual.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal