Rehost a FactoryTalk Optix Studio Pro entitlement
You can rehost the
FactoryTalk®
Optix Studio™
Pro entitlement by using either the FactoryTalk®
Optix Studio™
desktop application or the FactoryTalk® Optix™
landing page.Follow one of the following procedures to reallocate a
FactoryTalk®
Optix Studio™
Pro entitlement from a user to another.Rehosting from the desktop application
- Make sure that your device is connected to the Internet.
- Access theFactoryTalk® Optix Studio™desktop application.
- Click theLoginicon at the top right corner.
- On the drop-down menu, selectRehost entitlement.
Rehosting from the FactoryTalk® Optix™ landing page
FactoryTalk® Optix™
landing page- Make sure that your device is connected to the Internet.
- Access theFactoryTalk® Optix™landing page.
- Select .
- Click theRehostbutton located in the rightmost column next to theFactoryTalk® Optix Studio™Pro entitlement that you want to rehost.
Provide Feedback