Save a project
Save a project or Optix template locally, in a version control repository, on a network drive, or a
removable drive.
- Save a project using one of three ways:
- From the toolbar, selectSave.The project is saved to the same location from which you opened the project.
- From the toolbar, select the down arrow after
, select
Save As, and then inSave project as, save the project as either a project or an Optix template:- Name. Enter a new name.
- Save as type. Select eitherOptix projectto save the project with a .optix extension, orOptix templateto save the project with a .optixt extension.
- Location. Enter the location to save the project or Optix template.TIP: The location for saving a template is read-only. All templates are stored in C:\Users\UserName\Documents\RockwellAutomation\FactoryTalk Optix\ProjectTemplates and are prepended with template_.
- (optional) To encrypt project or Optix template passwords, custom objects that have thePasswordDataType, andYAMLfiles that represent the project information model, select the option next toSecrets Encryption Modeand then forNew projects secrets encryption, select either:
- Remote key store. Encrypt project secrets by using a remote key store. You need to be logged in toFactoryTalk Huband be a part of a relevant organization.
- User provided password. Encrypt project secrets with a password.
TIP: For more information about secrets encryption and the default project encryption for new projects, see Project secrets encryption and Set options. - SelectOK.
- From the toolbar, select .The project or Optix template is saved and a commit is made to the local version control repository. When you commit project changes for the first time, a Git repository initializes for the project.
repository
network drive
removable drive
Provide Feedback