Edit an Optix template
To edit a user-defined Optix template so that any new project created with the
template contains the revised content, open the Optix template and modify the content.
- In the main toolbar, select
Project.The Start page opens. - Open the Optix template by opening either:
- Recent template. SelectHomeor selectOpenand then selectRecentto select the Optix template to open.
- Remote template. SelectOpenand then selectRemoteto select the Optix template to open, or enter aRemote URLandLocationto select a remote Optix template.
TIP: For information on how to emulate Optix templates on client devices, see Add a target device. - Change the content in the Optix template.
- Save the Optix template with:
- The same name. From the toolbar, selectSave.
- A different name:
- Name. Enter the new name of the Optix template.
- Save as type. SelectOptix Template (*.optixt).
- Location. The location for templates is read-only.TIP: Optix templates are stored inC:\Users\Username\Documents\Rockwell Automation\\FactoryTalk Optix\ProjectTemplates. Optix template names are prepended withFTOptix_template_.
- (optional)Use Version Control. Select to track changes made to the Optix template and store the template in a Git repository.
- (optional)Encrypt secrets. Select to encrypt sensitive data contained in the Optix template.
- SelectOK.
- The same name and committed to the repository. From the toolbar, select .
- To close the Optix template, from the main toolbar, selectProject, and then on the Start page, selectClose Project.
Provide Feedback