Create a style sheet

Each project you create from a standard template includes a style sheet. You can create additional style sheets for the project.
TIP: Instead of creating your own style sheet from scratch, you can add a predefined style sheet. See Add a predefined style sheet. For example, you can add a dark style sheet.
  1. In
    Project view
    , right-click
    UI
    and select
    New
    Style sheet
    .
    StyleSheet
    #
    appears in
    Project view
    .
  2. (optional) Hover-over
    StyleSheet
    #
    , select
    Edit
    , and enter a new name for the style sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal