Data controls
    Use data controls objects to visualize data in your application interface. Get data from project nodes or a database.
| Object | Description | 
|---|---|
| Select items from a drop-down list at runtime. | |
| Select items from a list box at runtime. | |
| Display data in a table. | |
| Display trends that present values from one or more variables that are logged or read in real time. | |
| Display the value of two-dimensional variables in a graph. | |
| Display data in the form of a pie chart. | |
| Display data in the form of a bar diagram. | 
Provide Feedback