Parameters Not Reset When Set Defaults Most Executes
IMPORTANT:
The PowerFlex 20-HIM-A6/-C6S HIM User Manual, publication 20HIM-UM001, provides detailed instructions on using Human Interface Module capabilities, including, setting the
PowerFlex®
750-Series drive to factory settings. Port 0: Product Config File, Preferences Group
Number | Display Name | Full Name |
|---|---|---|
30 | Access Level | User Access Level |
31 | Language | Display Language |
46 | Velocity Units | Velocity Units |
Port 0: Product Config File, Control Config Group
Number | Display Name | Full Name |
|---|---|---|
33 | VoltageClass Cfg | Voltage Class Configure |
35 | Duty Rating Cfg | Duty Rating Configure |
Port 0: Product Config File, Port Mode Group
Number | Display Name | Full Name |
|---|---|---|
65 | Pri MtrCtrl Mode | Primary Motor Control Mode |
70 | Application Sel | Application Select |
Port 0: Product Config File, Option Cfg Group
Number | Display Name | Full Name |
|---|---|---|
80 | DCP Option | DC Precharge Option |
82 | TAM Option | Torque Accuracy Module Option |
Port 0: Feedback & I/O File, Command Group
Number | Display Name | Full name |
|---|---|---|
134 | DI EmergencyOVRD | Digital Input Emergency Override |
Port 0: Embedded ENET File, Address Config Group
Number | Display Name | Full Name |
|---|---|---|
300 | Net Addr Sel | Network Address Selection |
302 | IP Addr Cfg 1 | IP Address Configuration 1 |
303 | IP Addr Cfg 2 | IP Address Configuration 2 |
304 | IP Addr Cfg 3 | IP Address Configuration 3 |
305 | IP Addr Cfg 4 | IP Address Configuration 4 |
306 | Subnet Cfg 1 | Subnet Configuration 1 |
307 | Subnet Cfg 2 | Subnet Configuration 2 |
308 | Subnet Cfg 3 | Subnet Configuration 3 |
309 | Subnet Cfg 4 | Subnet Configuration 4 |
310 | Gateway Cfg 1 | Gateway Configuration 1 |
311 | Gateway Cfg 2 | Gateway Configuration 2 |
312 | Gateway Cfg 3 | Gateway Configuration 3 |
313 | Gateway Cfg 4 | Gateway Configuration 4 |
314 | Net Rate Cfg 1 | Net Rate Configuration 1 |
316 | Net Rate Cfg 3 | Net Rate Configuration 3 |
Port 0: Protection File, Overrides Group
Number | Display Name | Full Name |
|---|---|---|
454 | Emerg OVRD Mode | Emergency Override Mode |
455 | Emerg Prot OVRD | Protections Overriden by Emergency Override |
Parameter 0:457 [Purge Frequency]
ATTENTION:
Unintended parameter value can result due to This Port Only reset. Parameter 0:457 [Purge Frequency] is reset to the default value when a Set Defaults for This Port Only is applied to port 10 or port 11.
Peripheral Set Defaults Operation Resets Host Product
The parameters for some
PowerFlex®
750-Series option modules reside on the main control board of the host product. Because of this scheme, performing a Set Defaults operation for one of these peripheral devices resets the host product. The peripherals that behave in this way are listed in this table.Peripheral | Cat. No. |
|---|---|
11-Series I/O option modules | 20-750-1132C-2R |
20-750-1133C-1R2T | |
20-750-1132D-2R | |
22-Series I/O option modules | 20-750-2232C-2R |
20-750-2233C-1R2T | |
20-750-2232D-2R | |
Single incremental encoder option module | 20-750-ENC-1 |
Dual incremental encoder option module | 20-750-DENC-1 |
Provide Feedback