View Faults, Alarms, Events, and Exceptions
When a condition occurs, the drive records the occurrence in the fault, alarm, event, or exception queue. These queues are accessible through software or the HIM and provide you with a history of each type of occurrence. You can also access diagnostic file parameters for additional information.
- Port 0: Diagnostics File, Status Group
- Port 0: Diagnostics File, Fault/Alarm Info Group
- Port 10: Diagnostics File, Status Group
- Port 10: Diagnostics File, Fault/Alarm Info Group
- Port 13: Diagnostics File, Status Group
- Port 13: Diagnostics File, Fault/Alarm Info Group
Fault and Alarm Display Codes
Event numbers for faults and alarms are displayed in one of these formats.
- Port 00 (Host Drive) displays the event number only. For example, code 21 ‘Clr Fault Queue’ is displayed as: Fault Code 21.
- Ports 01 through 09 use the format PEEE, indicating port number (P) and event number (EEE). For example, code 1 ‘Analog In Loss’ on an I/O module installed in Port 4 is displayed as: Fault Code 4001.
- Ports 10 through 14 use the format PPEEE, indicating port number (PP) and event number (EEE). For example, code 37 ‘S OverTemp Alm’ on Port 14 is displayed as: Fault Code 14037.
HIM Fault Display
By default, the status bar flashes to alert the operator. To change the display flash mode, see the PowerFlex 20-HIM-A6 and 20-HIM-C6S HIM User Manual, publication 20HIM-UM001, for instructions.
The fault display screen displays the following information.
- Fault Code number
- Fault description
- Elapsed time (in hh:mm:ss format) from fault detection
Pop-Up/Flashing Fault Display Screen
Label | Name | Descriptions |
|---|---|---|
ESC | Escape | Reverts to the previous screen without clearing the fault. |
CLR | Clear | Removes the pop-up Fault Display screen from the display and clears the fault. |
Key | Name | Description |
|---|---|---|
Stop | Removes the pop-up Fault Display screen from the display and clears the fault. |
Provide Feedback