Common Symptoms and Corrective Actions
These are symptoms you may experience with your drive and corrective actions to take.
Drive Does Not Start from Inputs Wired to the Terminal Block
Cause(s) | Indication | Corrective Action |
|---|---|---|
Drive is faulted | Flashing red status indicator | Clear fault.
|
Incorrect input wiring. See publication 750-IN111, for wiring examples.
| None | Wire inputs correctly. |
Incorrect digital input programming.
| None | Configure input function. |
Flashing yellow status indicator and ‘DigIn Cnfg B’ or ‘DigIn Cnfg C’ indication on LCD HIM. 10:355 [Motor Side Sts 2] shows type 2 alarm(s). | Resolve input function conflicts. | |
Terminal block does not have control. | None | Check 0:41 [Logic Mask]. |
Drive Does Not Start from HIM
Cause(s) | Indication | Corrective Action |
|---|---|---|
Drive is configured for 2-wire level control. | None | Change 0:101 [Digital In Cfg] to correct control function. |
Another device has Manual control. | None | — |
Port does not have control. | None | Change 0:41 [Logic Mask] to enable correct port. |
Drive Does Not Respond to Speed Command
Cause(s) | Indication | Corrective Action |
|---|---|---|
No value is coming from the source of the command. | LCD HIM Status Line indicates ‘At Speed’ and output is 0 Hz. | If the source is an analog input, check wiring and use a meter to check for presence of signal. |
Incorrect reference source has been programmed. | None |
|
Incorrect Reference source is being selected via remote device or digital inputs. | None |
|
Motor or Drive Does Not Accelerate
Cause(s) | Indication | Corrective Action |
|---|---|---|
Acceleration time is excessive. | None | Reprogram 10:1915/ 1916 [VRef Accel Timen]. |
Excess load or short acceleration times force the drive into current limit, slowing or stopping acceleration. | None | Check 10:354 [Motor Side Sts 1], bit 27 to see if the drive is in Current Limit. Remove excess load or reprogram 10:1915/1916 [VRef Accel Timen]. |
Speed command source or value is not as expected. | None | Check for the proper Speed Command using Steps 1 through 7 above. |
Programming is preventing the drive output from exceeding limiting values. | None | Check 10:1898 [Vel Limit Pos], 10:1899 [Vel Limit Neg], and 10:422 [Maximum Freq] to assure that speed is not limited by programming. |
Motor Operation Is Unstable
Cause(s) | Indication | Corrective Action |
|---|---|---|
Motor data was incorrectly entered or Autotune was not performed. | None |
|
Drive Does Not Reverse Motor Direction
Cause(s) | Indication | Corrective Action |
|---|---|---|
Digital input is not selected for reversing control. | None | Check that the DI Reversing function is correctly configured. |
Digital input is incorrectly wired. | None | Check digital input wiring. |
Direction mode parameter is incorrectly programmed. | None | Reprogram 10:930 [Direction Mode], for analog ‘Bipolar’ or digital ‘Unipolar’ control. |
Motor wiring is improperly phased for reverse. | None | Switch any two motor leads. |
A bipolar analog speed command input is incorrectly wired or signal is absent. | None |
|
Drive Stop Results in Decel Inhibit Fault
Cause(s) | Indication | Corrective Action |
|---|---|---|
The bus regulation feature is enabled and is halting deceleration due to excessive bus voltage. Excess bus voltage is normally due to excessive regenerated energy or unstable AC line input voltages. | Decel Inhibit fault screen. LCD Status Line indicates ‘Faulted.’ |
|
Internal timer has halted drive operation. |
Datalink Problems
Cause(s) | Indication | Corrective Action |
|---|---|---|
Another device is communicating with the processor. | None |
|
Provide Feedback