Requirements for Use Control
Product | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® Security softwareStudio 5000 Logix Designer® application | Yes | Configure FactoryTalk® Security to define policies, user groups, and other permission sets.
For more information, see the following:
|
Microsoft® Active Directory service | Yes | Active Directory is used to create and configure the policies for each user and user group.
For more information, see the following:
|
Secure DPI™ Ports | Yes | Applicable for I/O mode only: HIM and Communication option cards are connected to the drive through DPI ports and should be secured by configuring the mask parameters in the drive. After product commissioning, HIM should be either removed or set to read-only mode. To remove HIM, see instructions in the PowerFlex 20-HIM-A6 and 20-HIM-C6S HIM User Manual, publication 20HIM-UM001. Communication option cards should also be disallowed from controlling the logic command (start, jog, change of direction, and so forth) of the drive. The following mask parameters can be used to configure the control to logic command and to set read-only mode:
For more information, see CIP Security with Rockwell Automation Products, publication SECURE-AT001. Applicable for CIP Motion mode only: HIM can only be used for monitoring and cannot be used to control the drive or change configuration settings. For more information, see Integrated Motion on the EtherNet/IP Network: Configuration and Startup User Manual, publication MOTION-UM003. |
FactoryTalk® Policy Manager | Yes | FactoryTalk® Policy Manager is a secure configuration tool that is one of a set of products that Rockwell Automation® uses to implement CIP Security.CIP Security helps to provide a secure data transport across an EtherNet/IP network. Use FactoryTalk® Policy Manager software to create zones and turn on CIP Security to check for data integrity.
|
FactoryTalk® AssetCentre software | Yes | Configure and use the following:
For more information, see the following:
|
Syslog collector | Yes, if not using FactoryTalk® AssetCentre for logging | The Drive supports syslog event logging. Choose a syslog collector that supports the following:
IMPORTANT: The drive sends events to a syslog collector through its Ethernet port. The Ethernet port must be connected to the same network as the syslog collector. To set the IP address of the syslog collector, use FactoryTalk® Policy Manager software. For more information, see CIP Security with Rockwell Automation Products Application Technique, publication SECURE-AT001.To view a list of syslog messages and their descriptions, see the PowerFlex Drives with TotalFORCE Control Conditions Reference Data, publication 750-RD102. |
Secure Hardware Input Device | Yes, if the hardware input device is programmed to control critical function | Hardware input devices such as push buttons can be programmed to control critical functions such as start, stop, and reset via discrete I/O port available on the drive. To apply security measures, for example, limiting physical access on such hardware input devices to prevent accidental or intentional alteration of drive critical function state. |
Provide Feedback