Requirements for Identification and Authorization
Product | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® Security softwareStudio 5000 Logix Designer® application | Yes | Configure FactoryTalk® Security to define policies, user groups, and other permission sets.
For more information, see the following:
|
Microsoft® Active Directory service | Yes | Active Directory is used to create and configure the policies for each user and user group.
For more information, see the following:
|
Provide Feedback