Checklist for Safety Outputs
For programming or startup, an individual requirement checklist must be completed for every safety output in the system. This method is the only way to make sure that the requirements are fully and clearly implemented. This checklist can also be used as documentation on the connection of external wiring to the application program.
✔ | Output Device Requirements |
|---|---|
Have you followed installation instructions and precautions to conform to applicable safety standards? | |
Have you performed project validation tests on the system and devices? | |
Have you uploaded and compared the configuration of each device to the configuration sent by the configuration tool? | |
Have you verified that test outputs are not used as safety outputs? | |
Are devices wired in compliance with the target standard and required safety level? | |
Have you verified that the electrical specifications of the output and the actuator are compatible? |
Provide Feedback