Print a report

You can print an individual report for the selected
Controller Organizer
component. You can also print multiple reports.
Controller Organizer
items for which you can print reports include:
  • Individual modules (I/O module, drive, or HMI)
  • Modules wired to a network (Ethernet, ControlNet, or DeviceNet)
  • Backplane modules
  • Tasks
  • Programs
  • Equipment Phase
    s
  • Equipment Sequence
    s
  • Routines (including external routines)
    TIP: Backplane module reports include properties for the communication module in the backplane. All other component reports only display data for the selected component, not its communication modules.
To print a report
  1. In the
    Controller Organizer
    , select the desired item.
    TIP: When a properties dialog is displayed and is the active window, you can print properties regardless of what is selected in the
    Controller Organizer
    .
  2. Select
    File > Print
    . You can also right-click the module and select
    Print
    or press
    Ctrl+p
    . The
    Print - Controller Organizer
    dialog box appears.
  3. Select
    Print Options
    . The
    Print Options
    dialog box appears.
  4. Select the item's applicable Properties option. For example, if you have selected a component under I/O Configuration in the Controller Organizer, select
    Module Properties
    . For tasks, programs, Equipment Phases, Equipment Sequences, or routines, select
    Task Properties
    ,
    Program Properties
    ,
    Equipment Phase Properties
    ,
    Equipment Sequence Listing
    , or
    Routine Properties
    respectively.
    If you have activated the Equipment Phase, the Program/Phase Properties option appears for Equipment Phases.
  5. Select
    OK
    to close the
    Print Options
    dialog box.
    To print a report without first displaying the
    Print - Controller Organizer
    dialog box, select the Print icon in the main toolbar.
  6. On the
    Print - Controller Organizer
    dialog box, select the printer, the pages to be printed, and the number of copies, and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal