Failed to set Dialog Field Name alarm value

In the alarm tab of the
PID configuration
dialog box, there is an error in the specified alarm field. The minimum value specified is greater than the maximum value. Enter a minimum value that is less than the maximum value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal