Select the Catalog Number as the data source

Using the
Motor
tab, specify where the motor configuration values are originating by selecting a motor by catalog number from the Motion Database.
To select the Catalog Number as the data source:
  1. In the
    Axis Properties
    dialog box, in the
    Categories
    pane
    ,
    click
    Motor
    .
  2. In the
    Motor Device Specification
    area, from the
    Data Source
    list, click
    Catalog Number
    .
  3. Click
    Change Catalog
    .
  4. In the
    Change Catalog Number
    dialog box, select a motor and click
    OK
    . The
    Nameplate/Datasheet - Phase to Phase
    parameters are populated with the parameter information for the selected motor.
  5. Click
    Apply
    to apply the changes.
    Tip:
    When using a motor catalog number as the data source, default values, for example, gains and dynamics, are automatically set based on the
    Application Type and Loop Response
    settings from the
    General
    tab. Using default values minimizes the need for adjusting these parameters using autotune, manual tune, and the manual setting of these parameters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal