Input/Output Instructions
The input/output instructions read or write data to or from the controller or a block of data to or from another module on another network.
Available Instructions
Ladder Diagram and Structured Text
Function Block
Not available
If you want to: | Use this instruction: |
|---|---|
Send data to or from another module | MSG |
Get controller status information | GSV |
Set controller status information | SSV |
Send output values to an I/O module or consuming controller at a specific point in your logic Trigger an event task in another controller | IOT |
Provide Feedback