Attach to Phase (PATT)
This instruction applies to the Compact GuardLogix 5370 and Compact GuardLogix 5380, CompactLogix 5370, CompactLogix 5380, and CompactLogix 5480, ControlLogix 5570 and ControlLogix 5580, and GuardLogix 5570 and GuardLogix 5580 controllers.
TIP:
When using this instruction with ControlLogix redundancy system, outputs controlled by this instruction may not be bumpless during redundancy switchover, if the instruction and phase program are not scheduled in the highest priority task.
- Prevent another program orFactoryTalk Batchsoftware from commanding an equipment phase.
- Make sure another program orFactoryTalk Batchsoftware does not already own an equipment phase.
The PATT instruction lets a program take ownership of an equipment phase.
- Ownership is optional. As long as an equipment phase has no owners, any sequencer (program in the controller,FactoryTalk Batchsoftware) can command an equipment phase.
- FactoryTalk Batchsoftware always takes ownership of an equipment phase.
- Once a sequencer owns an equipment phase, no other sequencer can command the equipment phase.
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
PATT(Phase_Name,Result);
Operands
Ladder Diagram
Operand | Type | Format | Description |
|---|---|---|---|
Phase Name | PHASE | Name of the equipment phase | Equipment phase to own. |
Result | DINT | immediate tag | To let the instruction return a code for its success or failure, enter a DINT tag in which to store the result code. Otherwise, enter 0. |
Structured Text
The operands are the same as those for the Ladder Diagram PATT instruction.
Guidelines for using the PATT Instruction
Guideline | Details | |
|---|---|---|
Consider ownership if have multiple sequencers that use a common equipment phase. | Ownership makes sure that a program can command all the equipment phases it needs and locks out any other sequencers. | |
If using: | Then: | |
FactoryTalk Batch software to also run sequences within this controller | Before executing the sequence (process), take ownership of all the equipment phases that the sequence uses. | |
Multiple programs to command the same equipment phase | ||
None of the above | No need to own the equipment phases. | |
Remember that Logix Designer overrides the controller. | Regardless of whether a program or FactoryTalk Batch software owns an equipment phase, the option exists to use Logix Designer to override ownership and command the equipment phase to a different state. | |
This: | Overrides this: | |
Logix Designer | Controller (internal sequencer), FactoryTalk Batch software (external sequencer) | |
Controller (internal sequencer) | None | |
FactoryTalk Batch software (external sequencer) | None | |
Use the Result operand to validate ownership. | Use the Result operand to get a code that shows the success or failure of the PATT instruction. To interpret the result code, see the PATT Result Codes | |
Avoid or plan for a result code = 24582. | On each execution, the PATT instruction tries to take ownership of the equipment phase. Once a program owns an equipment phase, another execution of the PATT instruction produces a result code = 24582. When using a PATT instruction, either:
| |
When the sequence is done, relinquish ownership. | To relinquish ownership, use a Detach from Equipment Phase (PDET) instruction. | |
PATT Result Codes
If assigning a tag to store the result of a PATT instruction, the instruction returns one of these codes when it executes:
Code (Dec) | Description |
|---|---|
0 | The command was successful. |
24579 | Logix Designer or HMI already owns equipment phase. The caller is attached to the equipment phase, but it is not the current commanding owner.
|
24582 | The program already owns the equipment phase. |
24593 | One of these already owns the equipment phase:
|
24594 | The equipment phase is unscheduled, inhibited, or in a task that is inhibited. |
Affects Math Status Flags
No
Major/Minor Faults
None. See
Index Through Arrays
for operand-related faults.Execution
For Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic, it will execute. All Conditions below the thick solid line can only occur during Normal Scan mode.
Condition/State | Action Taken |
|---|---|
Prescan | No action taken. |
Postscan | No action taken. |
EnableIn is false | No action taken. |
EnableIn is true | The instruction executes as described above. |
Example
Ladder Diagram
If
Step.1
= 1 (first step in the sequence) thenEach PATT instruction tries to take ownership of an equipment phase.
If the Result of a PATT instruction = 0 or 24582 (the program owns the equipment phase), then
A bit within the
Ownership
tag = 1. (In the Ownership
tag, each equipment phase is assigned a bit.)If
Ownership
= 3 (The program owns both equipment phases as shown by bits 0 and 1), thenDone
= 1. (This signals the sequence to go to the next step.)
Structured Text

Number | Description |
|---|---|
![]() | At the first step in the sequence, the Take_Ownership action tries to take ownership of two equipment phases that the sequence uses. |
![]() | Action_009 checks that the program owns the equipment phases. If the Result of each PATT instruction = 0 or 24282 (the program owns the equipment phase), then a bit within the Ownership tag = 1. (In the Ownership tag, each equipment phase is assigned a bit.) |
![]() | If the Ownership = 3 (The program owns both equipment phases as shown by bits 0 and 1.), then the SFC goes to the next step. |
Provide Feedback