Animate the side menu
- Select the side menu shape, and inPropertiesselect, and select
Variable. - Rename the new variable toSideMenuActive
- Change the variable data type to Boolean.
- Select the button, and inEvents, next toMouseClick Event:
- Select.

- Select .
- ChooseSelect.
- InEvents, next toVariableToModifyselect.
Add Dynamic Link - Select .
- Select the side menu, and inPropertiesnext toLeft marginselect.
Add Dynamic Link - In theAdvancedtab, next toLeft margin:
- Select.

- SelectConditional converter.
- SetFalse valueto-140
- Next toCondition Dynamic linkselect.
Add Dynamic Link - Select .
- SelectOK.
Provide Feedback