Create an event logger
Create a logger that monitors the current temperature.
- InProject view, right-clickLoggersand select .
- Configure events:
- InProperties, next toEvent configurations, select.

- SetListen subtreetoFalse.
- Set theEvent typetoAlarmConditionType.
- InProperties, double-clickEventLogger1
- In the editor, select these variables:
- .
- .
- .
- .
- .
- .
- In the editor, selectApply.
- Create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
Provide Feedback