Debug NetLogic locally with Visual Studio
Debug a local project with design-time and runtime NetLogics by using
Visual Studio®
.Prerequisites
- Download, install, and setVisual Studioas the default code editor. See Set the default code editor.
- Learn about debugging inVisual Studio. See First look at the debugger - Visual Studio (Windows) | Microsoft Learn.
- To debug NetLogic locally with Visual Studio
- From the main toolbar, select
Open .NET Solution.Visual Studioopens. - Either:
- Debug a runtime NetLogic. Run theFactoryTalk Optix Applicationand then inVisual Studio, attach to theFTOptixRuntimeprocess. See Deploy a FactoryTalk Optix Application.
- Debug a design-time NetLogic. InVisual Studio, attach to theFTOptixStudioprocess and execute the design time NetLogic. See Run a NetLogic at design time.
- Stop the debugging process, edit the code, and repeat the procedure.
Provide Feedback