Asynchronous task
    Create asynchronous tasks to run code asynchronously. 
Classes
      FactoryTalk Optix Studio
 provides C# class specifications that exhibit the constructors that you can use for creating asynchronous tasks. The constructors are based on the .NET Framework C# System.Threading.Tasks.Task
 class, which represents an asynchronous task. See Task Class.You can use these classes to create asynchronous tasks:
- PeriodicTask
- A task that runs code at regular time intervals. See Constructor: PeriodicTask(action, periodMilliseconds, excutingNode).
- DelayedTask
- A task that runs code after a time delay. See Constructor: DelayedTask(action, delayMilliseconds, executingNode).
- LongRunningTask
- A task that requires significant time or CPU resources. See Constructor: LongRunningTask(action, executingNode).
     TIP: 
    You can also use C# async methods to run asynchronous code. C# async methods cannot interact with the project model. For example, C# async methods should not read or write a model variable. To modify the project model asynchronously, use the 
PeriodicTask
, DelayedTask
, LongRunningTask
 classes to construct asynchronous tasks.Provide Feedback