HTTP methods
    The REST API Client NetLogic exposes these HTTP methods: GET, POST, PUT.
Get
      Use the GET method to request data from an API endpoint.
        
  
    
| Argument | Description | 
|---|---|
| apiUrl | Address of an endpoint to access the API. | 
| queryString | Arguments to pass to the API endpoint. | 
| bearerToken | Token to authenticate the request. | 
Post
      Use the POST method to send data to an API endpoint and create a resource on the server.
        
  
    
| Argument | Description | 
|---|---|
| apiUrl | Address of an endpoint to access the API. | 
| requestBody | Data to send to the server behind the API endpoint. | 
| bearerToken | Token to authenticate the request. | 
| contentType | The original media type of the resource. | 
Put
      Use the PUT method to send data to an API endpoint and create or replace a resource on the server.
        
  
    
| Argument | Description | 
|---|---|
| apiUrl | Address of an endpoint to access the API. | 
| requestBody | Data to send to the server behind the API endpoint. | 
| bearerToken | Token to authenticate the request. | 
| contentType | The original media type of the resource. | 
Provide Feedback