Create an OPC UA method callable by an external OPC UA Client
    Create an OPC UA method callable by an external OPC UA client and then edit its code
      in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
- To create an OPC UA method callable by an external OPC UA Client
- Create an object type. See Create an object type.
- In theProject viewpane, right-click the object type and selectAdd custom behavior.
- Right-click the object type and selectEdit with .NET code editor (external).The external code editor opens. The following code is added in the NetLogic:[CustomBehavior] public class testTypeBehavior : BaseNetBehavior { public override void Start() { // Insert code to be executed when the user-defined behavior is started } public override void Stop() { // Insert code to be executed when the user-defined behavior is stopped } #region Auto-generated code, do not edit! protected new testType Node => (testType)base.Node; #endregion }
In the code editor, develop the method. For a complete example, see Develop a method callable by external OPC UA clients.
Provide Feedback