Session nodes
The
{Session}
alias points to the Session
node for the current runtime session. FactoryTalk Optix Studio
automatically creates dynamic links with the nodes inside of the Session
node.Session nodes include:
Node | Description |
|---|---|
Groups | Groups can be defined and used in the project. Each group displays a value:
|
MeasurementUnits | List of the available amounts. Each amount has properties based on the locale:
|
Locale | Array of session locale IDs. This node specifies all of the locales supported by the user interface. |
User | Properties for the user:
|
Roles | Roles can be defined and used in the project. Each role displays a value:
|
Provide Feedback