Configure OPC UA client certificates and keys
Edit the properties of an OPC UA client object to configure the public certificates and private keys.
Prerequisites
- InProject view, select anOPCUAClientobject.
- InProperties, next toClient certificate file, selectBrowse.
- InSelect file:
- If the certificate is listed, select the certificate and chooseSelect.
- If the certificate is not listed:
- Select.
Import file(s) - Select the certificate. For more information, see Certificates and keys location.
- ChooseSelect.
- InProperties, next toClient private key, selectBrowse.
- InSelect file:
- If the private key is listed, select the private key and chooseSelect.
- If the private key is not listed:
- Select.
Import file(s) - Select the private key. For more information, see Certificates and keys location.
- ChooseSelect.
Provide Feedback