Add a scale line pen
Add a scale line pen to visualize the distance between two variable values.
Prerequisites
- To add a scale line pen
- Create two variables of the Number data type.For more information, see Variables.
- InProperties, next toPens, selectand select
Scale line pen. - Create dynamic links between theXandYproperties and the variables.For more information about dynamic links, see Create dynamic links.
scale line
Provide Feedback