Add a polygon pen
Add a polygon pen to visualize the distance between values of an array variable.
Prerequisites
- Add a polygon pen
- InProject view, select or create an array variable of the Number data type.For more information, see Variables.For example, create a variable of the Number[2,3] data type.
- InProject view, select or create anXYChartobject.
- InProperties, next toPens, selectand select
Polygon line pen. - Create a dynamic link betweenPoint arrayand the array variable.For more information about dynamic links, see Create dynamic links.
polygon
Provide Feedback