Configure a label
Add a label object and edit its properties.
- InProject view, inUI, right-click a container to contain the label, and then select .
- (optional) InProject view, hover-overLabel, select#, and enter a new name for the label.

- InProperties, adjust the text and font of the label:
- Text. Text to display in the label.TIP:To display dynamic text, create a dynamic link betweenTextand a variable. Use a String formatter to customize the displayed variable value. For more information, see Dynamic links and String formatter.To insert a new line of text, while editingText, press+Alt. For more information, see Keyboard shortcuts.Enter
- Text color. Color of the text to display.
- Text horizontal alignment. Text position on the x-axis.
- Text vertical alignment. Text position on the y-axis.
- Word wrap. Wrap text if the text is larger than the container.
- Text trimming. Trim text and display...to indicate that label text is too long to fit the container.TIP:Word wraptakes precedence overText trimming.
- Font family. Font family of the label.
- Font size. Size of the label font.
- Font weight. Weight of the label font.
- Font italic. Italicize label font.
- Font underline. Underline label font.
label
multiline
multi-line
multiple lines
Provide Feedback