Key-value converter
Convert the value of the source to its corresponding parent value based on a table of key-value pairs. The key-value converter converts heterogeneous data, such as a color to value.
Key-value editor
You can open the key-value editor by selecting
next to the key-value converter in advanced dynamic link editor.


Item | Name | Description |
|---|---|---|
![]() | Converter path | The path to the converter. |
![]() | ![]() | Adds a key-value table row. |
![]() | Delete | Deletes the selected key-value table row. |
![]() | Data type | Indicates the data type of keys or values. Select to choose a different data type. |
![]() | Key | A converter key (source value). |
![]() | Value | A value that corresponds with the key in the same row (output value).
TIP:
The value in the first row is the default value. If the source value does not correspond with any converter key, the converter returns the default value.
|
Properties
Property | Description |
|---|---|
Mode | The direction of the dynamic link:
|
Source
A variable with a value corresponding to a key.
Output
The value associated with the key in the map.
Example

key value
key value converter
key value editor
Provide Feedback







Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.