Keyboard navigation in Ladder Editor Toolbox
Certain keys navigate elements in the Ladder Editor
Toolbox
: Key | Sets focus on |
|---|---|
Up Arrow | Previous element in the Toolbox. |
Down Arrow | Next element in the Toolbox. |
Tab | Next element or category in the Toolbox. |
Shift+Tab | Previous element or category in the Toolbox. |
Esc | Removes focus from the Toolbox. |
Enter | Expands the selected Toolbox category or adds the selected element to the ladder diagram. Added items appear to the right of the selected item in the ladder diagram and wraps the rung as necessary. Added rungs appear below the selected rung. Select the END rung and then select Enter to have the new rung appear above the END rung. |
Page Down | Next view of items in the Toolbox. |
Page Up | Previous view of items in the Toolbox. |
Provide Feedback