Define a new Add-On Instruction
Create an Add-On Instruction to define a single instruction that contains commonly used logic. Add-On Instructions contain parameters and tags and the logic contained in standard ladder diagram.
Add-On Instructions appear in
Toolbox
for use throughout the project. Add an Add-On Instruction in Library
to reuse Add-On Instructions to provide consistency across the project or multiple projects.- On the explorer bar, select
Library. - InLibrary, select the Add-On Instruction item.
- From theLibrarymenu
, select New add-on instruction. - InNew add-on instruction, complete:
- Name. Type a unique name for the Add-On Instruction. Names must start with a letter or underscore and can contain up to 40 characters.
- Description. Enter the behavior of the Add-On Instruction. Descriptions contain up to 256 characters.
- Type. Select the language type of the main logic of the Add-On Instruction -- ladder diagram.
- Version number. Enter the major, minor, and build numbers of the Add-On Instruction.
- Version note. Enter additional information about this version.
- Vendor. Type the name of the vendor who owns the Add-On Instruction.
- (Optional) Select the items to open when the Add-On Instruction is created:
- Open definition. Open the definition of the Add-On Instruction.
- Open tags & parameters. Open the Tags and parameters tab for the Add-On Instruction.
- Open logic. Open the Ladder Editor for the Add-On Instruction.
- SelectCreate. The Add-On Instruction appears inLibrary. TheParameter & TagsandLogicitems appear in the data structure of the Add-On Instruction.TIP:
- The Add-On Instruction appears in the specified category inToolbox.
- A user-defined data type named (Name_AOI)_TYPE appears inLibraryunderDate TypesandAdd-On Defined.
- To open the Tag Editor for the Add-On Instruction, inLibraryselect the Add-On Instruction and then in theLibrarytitle bar, selectView
tags and parameters: (name)or double-click the user-defined data type named (Add-On Instruction name)_TYPE. - The Add-On Instruction has a parameter that executes the instruction and a read-only EnableOut parameter that updates the output of the instruction.
Provide Feedback