Apply a permission set to a routine

Apply a permission set to control access to a specific routine. Permission sets can be applied only when the overall project has been secured.
The security settings that you apply override and operate instead of any security policy applied to the overall project. Permission sets are maintained using the
FactoryTalk Administration Console
.
Tip:
To apply a permission set to a component, users must have Component: Modify Permission Set privileges, which are configured in
FactoryTalk Security
.
To apply a permission set to a routine:
  1. In the
    Controller Organizer
    or the
    Logical Organizer
    , right-click the routine and select
    Properties
    .
  2. In the
    Routine Properties
    dialog box, in the
    Permission Set
    control, select a permission set to apply.
  3. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal