The process timed out

Certain commands, such as the Motor/Encoder Test, time out if the command cannot be completed in two seconds. Check motor connections to make sure that the motor commands are connected correctly.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal