Hide/Show Wire command

Choose this command to hide/display the selected wire. A "to" arrow and a "from" arrow are displayed at the ends of the hidden wire, as well as:
  • the name and cross reference grid location of the element the wire is going to
  • the name and cross reference grid of the element the wire is coming from
When you position your cursor over the cross reference grid location, the location is underlined and the pointer changes to a pointing hand (as in a web browser). Clicking on the left mouse button allows you to navigate to the other end of the hidden wire.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal