Import and export
Use the import/export feature to import into or export out of a project. The
Logix Designer
application provides five different Import/Export file formats:- Full project exported to ASCII text file (.L5K, or to an Extensible Markup Language (XML) formatted file .L5X),
- Tag definitions and program documentation exported to ASCII text files in a Comma Separated Value (CSV) or Tab Separated Value (.TXT) format, and
- Import and Export these components in an Extensible Markup Language (XML) formatted file (L5X):
- Programs & Equipment Phases
- Routines & Phase State Routines (any language)
- Logic (Ladder Diagram Rungs only)
- User-defined Data Types (data types and custom Strings)
- Add-On Instructions
- Trends
- Tag-based alarms
- Modules
- Import or export hardware diagrams to or from a standard file type to share data between different software applications and theLogix DesignerProfessional Edition using these formats:
- Web Ontology Language (OWL)
- AutomationML (AML)
The import/export feature uses these file types:
.L5K and Files
An ASCII representation of the data for an entire project and, when imported, creates a new project file or overwrites an existing project file.
.CSV Files
A comma-separated text file containing the tags and logic comments. Export various object descriptions to a .CSV file to create, edit, translate, and spell check descriptions with offline tools, such as Microsoft Excel. When importing the .CSV file, the system merges that description into the
Logix Designer
application database.Export a .CSV file that contains as ASCII representation of tag information. Furthermore, import from a .CSV file and modify or add tag information to an open project.
For more information about importing and exporting a .CSV file, see
About the Import/Export Comment Data Feature
..TSV Files
A tab-separated text file containing the tags and logic comments. Similar to the .CSV file format, except values are separated by tabs instead of commas.
.L5X Files
An Extensible Markup Language (XML) formatted file. These files can contain an export of the entire project or an export of selected components (and component references).
.RDF files
AutoCAD Electrical
For AutoCAD Electrical, use the Rockwell Automation Data Adapter to exchange data between the
Logix Designer
application version 32.00.00 and AutoCAD Electrical versions 2014 through 2018. Data Adapter is a tool used to translate Rockwell Automation hardware data in OWL (.rdf) format for auto generation of two-dimensional footprint and PLC I/O schematic drawings in AutoCAD Electrical. Download the Data Adapter tool from Rockwell Automation's Product Download and Compatibility Center (PCDC).This workflow shows the supported process for bidirectional data exchange from
Studio 5000
applications to AutoCAD Electrical applications.
.AML files
EPLAN Electric P8
For EPLAN Electric P8, use AML data files (.aml) and associated PLC data import/export workflows to exchange data between the
Logix Designer
application version 32.00.00 and EPLAN Electric P8 version 2.7 and later.This workflow shows the process for data exchange from supported
Studio 5000®
applications to the EPLAN Electric P8 application when starting the data exchange within Studio 5000
.
This workflow shows the process for data exchange from the EPLAN Electric P8 application to supported
Studio 5000
applications when starting the data exchange within EPLAN.
Initiate the import of components and logic comments as follows:
- From the Controller Organizer, import a program, equipment phase, routine or phase state routine, Add-On Instruction, user-defined data type, string type, or trend by right-clicking on the component’s folder and accessing the import option from the context menu.
- From the Ladder Editor, import ladder rungs by right clicking on a rung header and selectingImport Rungs.
- From the mainFilemenu, selectImport Componentand then select the type of component to import.
- From the mainToolsmenu, selectImportand then select to import tags and logic comments or components.TIP:When exporting a component, make sure to select the component to be exported.
- From theSelect Project Controllerdialog box, select a project controller for the CAD tool.
When importing a component, make sure to select the container where that component should go (for example, to import a program, select the task where the program belongs).
Note that some of the options appear dimmed for:
- Safety tasks or when the project is safety secured
- Online in Run mode
- When activation for a component or permission to create or modify a component is not present
- The controller is online with an Add-On Instructions, or the routine or Add-On Instructions is source protected
- In Hard Run
- When the component type does not exist in the project
Safety Mapped Tags
When importing safety components while the controller is online, safety tag mapping is not exported or imported. When importing components, if tag mapping is required, map the tags after the import is completed.
Project Documentation
Projects may now contain comments and descriptions in multiple languages. Exports from a multi-language project include all languages existing in the project (for the components exported).
Imports also support multiple languages. When importing into a multi-language project:
- All languages in a multi-language export are imported.
- Prompt appears to specify the language of a single-language export.
When importing into a single-language project:
- Prompt appears to select one of the languages in a multi-language export file to import.
- The documentation in a single-language export file are imported.
Languages are identified uniquely by appending a colon and the language code to the existing .L5X token. For example, the United States English token is appended as :en-US. For more information about the Project Documentation Languages feature, refer to
About Project Documentation Languages
.External Access
When importing from an .L5K file or tag/logic component import from .CSV or .TXT files, the
Logix Designer
application verifies that the imported External Access value is valid and compatible with its tag. This table summarizes all incompatible External Access values that may result when modifying an .L5K, .L5X or .CSV file outside of the application and then trying to import the file:
Tag Type/Usage | Incompatible External Access Values |
InOut Parameter | Read/Write Read Only None |
EnableIn and EnableOut Parameter | Read/Write None |
PLC-5® / SLC™ , or PLC-2® mapped tags | None |
If importing tags with no External Access value specified, these default values are used:
Object Name | Default External Access during Import |
Controller and Program standard tags | Read/Write |
All Safety tags | Read/Write |
Add-On Instruction local tags | Read/Write |
Add-On Instruction input parameters | Read/Write |
Add-On Instruction Output, EnableIn, and EnableOut parameters | Read Only |
Add-On Instruction InOut parameters | N/A |
Equipment Phase Output parameter | Read Only |
Members of all data types | Read/Write |
Alias tag | External Access value of its target |
OPC UA Access
Tag Type/Usage | Incompatible OPC UA Access Values |
Program Output Parameter | Read/Write |
Program InOut Parameter | Read/Write Read Only |
Safety controller and program scope tags | Read/Write |
Const controller and program scope tags | Read/Write |
If you import controller or program-scope non-alias tags with no OPC UA Access value specified, the default value for OPC UA Access is None.
Provide Feedback