Equipment phases

The equipment phase is the smallest building block used by the
Equipment Phase
Manager
.
Within the
Logix Designer
application, an equipment phase functions much like a program. In this sense, equipment phases:
  • Can be executed within any task, except for Safety tasks.
  • Contain and execute multiple routines, including normal subroutines, prestate routines, fault routines, or routines containing the logic for different states of an equipment phase.
  • Can make use of the Max Scan and Last Scan timing functions.
  • Can have locally-scoped tags associated with them.
The behavior of the equipment phase is defined by its state machine. This state machine is a roadmap that describes how the equipment phase operates. The equipment phase enforces the transitions between states and runs the appropriate state routine when in an active state. For example, when the equipment phase is in the RUNNING state, it executes the Running routine. Likewise, if it is in the HOLDING state, it executes the Holding routine.
Create state routines for any of the active states of the equipment phase. Active states include:
  • ABORTING
  • HOLDING
  • RESETTING
  • RESTARTING
  • RUNNING
  • STOPPING
Logic for state routines
When the equipment phase state routines are created, write logic for each state in the Ladder Editor, the Sequential Function Chart Editor, the Structured Text Editor, or the Function Block Editor. This logic is referred to as phase logic. The
Logix Designer
application's
Equipment Phase
Manager
provides several instructions to support the development of phase logic.
Do not implement every active state. When you create an equipment phase, a controller scoped tag with the same name as the equipment phase is also created. This tag contains information on the state, sub state, owner, and other data related to the equipment phase. As the equipment phase executes, it updates this tag with its current state information.
The display of machine control states is driven from the data in the controller-scoped PHASE tag with the same name as the equipment phase. This controller-scoped tag has Producing and Standby bits to set in order to identify if the machine is in one of these sub states. Set and clear these bits at the appropriate time in the routine logic.
Applications that control equipment phases
Applications and programs can control the execution of equipment phases by sending them commands. These applications are referred to as sequencers. There are four types of sequencers that can command an equipment phase:
  • The
    Equipment Sequence
    Manager
    ,
    Logix Designer
    application's internal sequencer. The
    Equipment Sequence
    Manager
    arranges phases into sequences and uses instructions to command the phases.
  • The
    Logix Designer
    application's command toolbar and phase monitor window used to send commands to the equipment phase.
  • An External Sequencer, a PC-based application that commands the equipment phase through CIP messages.
  • HMI, a
    FactoryTalk View SE
    or ME station that commands the equipment phase through CIP messages.
Input and output parameter tags for equipment phases
Configure input or output parameter tags for an equipment phase. Parameter tags modularize the equipment phase and document the required or expected inputs and outputs. Parameter tags provide a mechanism for sequencers to store input values and retrieve output values while commanding the equipment phase. If the equipment phase has parameter tags, the sequencer typically performs these operations:
  • Take ownership of the equipment phase.
  • Write the input parameter values to the equipment phase’s tags.
  • Command the equipment phase (for example, START).
  • Wait for the equipment phase to complete (or reach another terminal state such as STOPPED or ABORTED).
  • Read the output parameter values from the equipment phase’s tags.
  • Release ownership of the equipment phase.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal