Change program schedule while online

This message appears while you are online in Remote Program, Remote Run, or Test mode, and you drag a program to or from the Unscheduled Programs folder (from or to one of the Tasks folders).
  • If you are dragging to a Task folder from the Unscheduled Programs folder and you click OK, the program you are dragging will become the last program in the Task's program schedule, and will no longer appear in the Unscheduled Programs folder.
  • If you are dragging from a Task folder to the Unscheduled Programs folder and you click OK, the program you are dragging will be removed from the Task's program schedule and will be placed in the Unscheduled Programs folder.
  • If you press Cancel, programs will remain where they were prior to the beginning of the drag-and-drop operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal