Keyboard shortcuts
FactoryTalk Optix Studio
supports these keyboard shortcuts.Global
Shortcut | Description |
|---|---|
F1 | Open FactoryTalk Optix Help. |
Ctrl C | Copy the selected item. |
Ctrl V | Paste the copied item into the selected location. |
Ctrl Z | Undo previous action. |
Ctrl Y | Redo previous action. |
Ctrl S | Save the current FactoryTalk Optix Application project. |
F5 | Run FactoryTalk Optix Application . For more information, see Deploy a FactoryTalk Optix Application. |
Ctrl Shift F | Find text in the current project. For more information, see Find text in a project. |
Ctrl Shift H | Find and replace text in the current project. For more
information, see Replace text in a project. |
Delete | Delete the selected item. |
Esc | Discard edits or close a dialog. |
Alt Enter | Add a new line. |
Enter | Interact with the selected item. |
Panes
The following shortcuts apply to panes in
FactoryTalk Optix Studio
. For more
information about FactoryTalk Optix Studio
panes, see FactoryTalk Optix Studio GUI.Shortcut | Description |
|---|---|
Up arrow | Select previous item. |
Down arrow | Select next item. |
Right arrow | Expand the selected item. |
Left arrow | Collapse the selected item. |
Alt Left
arrow | Select the previously selected item in Project
view . For more information, see Project view. |
Alt Left
arrow | Select the next item in Project view . For
more information, see Project view. |
Shift | Select all items between the selected item and the clicked
item. |
F2 | Rename the selected item. |
Localization dictionary
For more information about localization dictionaries and strings translation, see
Localization editor.
Shortcut | Description |
|---|---|
Ctrl A | Select all keys and values in the translation table. |
UI editor
The following shortcuts apply to the editor that allows you to arrange graphic
objects and create user interfaces for
FactoryTalk Optix Applications
. For more
information, see Editor.Shortcut | Description |
|---|---|
Up arrow | Move the selected object up on the grid. |
Down arrow | Move the selected object down on the grid. |
Left arrow | Move the selected object left on the grid. |
Right arrow | Move the selected object right on the grid. |
Shift Up arrow | Move the selected object up and align the object to the
grid. |
Shift Down
arrow | Move the selected object down and align the object to the
grid. |
Shift Left
arrow | Move the selected object left and align the object to the
grid. |
Shift Right
arrow | Move the selected object right and align the object to the
grid. |
Provide Feedback