CLI commands
FactoryTalk Optix Studio
includes these command-line interface (CLI)
commands.
TIP:
The following commands assume that you installed
FactoryTalk Optix Studio
in the default
location. If you selected a custom location for your FactoryTalk Optix Studio
installation, modify the paths accordingly. To shorten the commands and invoke the executable with
FTOptixStudio
, add a system environment variable or navigate to
the FactoryTalk Optix Studio
installation directory.
TIP:
The
--help
,
-h
, and --version
commands take
precedence over other commands. --help
and
-h
take precedence over
--version
.open
Use the
open
command to open a project in FactoryTalk Optix Studio
."C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" --open
project_to_open
[--silent]Parameter | Importance | Description |
|---|---|---|
version | Required | Folder name that reflects the installed FactoryTalk Optix Studio
version. |
project_to_open | Required | Path to the OPTIX file of the project to
open. |
--silent | Optional | Make the command output non-verbose in the command prompt. |
new
Use the
new
command to create a project."C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" --new
project_to_create
path
[-e | --encrypt-secrets]
[--template=template
]
[--main-window-width==width
]
[--main-window-height==height
] [-l |
--in-project-location] [--silent]Parameter | Importance | Description |
|---|---|---|
version | Required | Folder name that reflects the installed FactoryTalk Optix Studio
version. |
project_to_create | Required | Name for the project. |
path | Required | Location for the project. |
-e or
--encrypt-secrets | Optional | Encrypt secrets in the project. |
--template= template | Optional | Name of the template to use for the project. The allowed values for template are:
|
--main-window-width= width | Optional | Width for the main window in pixels. The default width is
400 pixels |
--main-window-height= height | Optional | Height for the main window in pixels. The default height is
400 pixels |
-l or
--in-project-location | Optional | Create the project directly under
path |
--silent | Optional | Make the command output non-verbose in the command prompt. |
connect
Use the
connect
command to connect FactoryTalk Optix Studio
with an endpoint."C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" --connect
endpoint
[--silent]Parameter | Importance | Description |
|---|---|---|
endpoint | Required | The IP address of the endpoint to connect to. |
--silent | Optional | Make the command output non-verbose in the command prompt. |
deploy
Use the
deploy
command to deploy a FactoryTalk Optix Application
to a local device.Consider the following when working with the
deploy
command:- You need to perform any necessary versioning operations before theFactoryTalk Optix Applicationdeployment.
- You need to ensure that theFactoryTalk Optix Applicationbuilds without errors before the deployment.
- You can only deployFactoryTalk Optix Applicationsto local devices.
- You cannot deployFactoryTalk Optix Applicationswith encrypted secrets.
"C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" deploy
project_to_deploy
--ip-address=ip_address
--username=username
[--thumbprint=certificate_thumbprint
]
[--disable-project-encryption] [--disable-source-project-transfer]
[--transfer-application-files] [--transfer-optimized-project]
[--silent]Parameter | Importance | Description |
|---|---|---|
version | Required | Folder name that reflects the installed FactoryTalk Optix Studio
version. |
project_to_deploy | Required | Path to the OPTIX file of the project to
deploy. |
ip_address | Required | IP address of the target device to deploy the FactoryTalk Optix Application to. |
username | Required | Username for logging on to the target device
IMPORTANT:
Specify user password
as a
OPTIX_STUDIO_DEPLOYMENT_PASSWORD
system environment variable. |
--thumbprint= certificate_thumbprint | Optional | Provide certificate thumbprint of the target FactoryTalk Optix
Application Update Service to prevent the need to interact with
the trust dialog. The trust dialog displays only for the first deployment. Ensure that the FactoryTalk Optix Runtime Tools and Update
Service are installed. Then, you can obtain the thumbprint by
running this command openssl x509 -fingerprint -in
UpdateServicePath /PKI/Own/Certs/FTOptixApplication.der
-inform DER -nooutwhere UpdateServicePath is the installation
directory of the FactoryTalk Optix Application Update
Service. |
--disable-project-encryption | Optional | Disable project encryption. |
--disable-source-project-transfer | Optional | Disable the transfer of the source project to the target
device.
IMPORTANT:
You can only transfer
source projects to Windows target devices.
|
--transfer-optimized-project | Optional | Optimize the project before its transfer. Optimized projects:
You cannot optimize projects containing OPC UA servers that expose the entire model
or at least one tag. |
--silent | Optional | Make the command output non-verbose in the command prompt. |
export
Use the
export
command to export a FactoryTalk Optix Application
to a file."C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" export
project_to_export
--platform=platform
--location=location
[--silent]Example:
"C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" deploy "D:\Device Sizing
Tool\Projects\BlankProject\BlankProject.optix" --ip-address=172.19.16.187
--username=adminConsider the following when working with the
export
command:- You need to ensure that theFactoryTalk Optix Applicationbuilds without errors before the export.
- You cannot set passwords for exportedFactoryTalk Optix Applications.
- You cannot exportFactoryTalk Optix Applicationswith encrypted secrets.
Parameter | Importance | Description |
|---|---|---|
version | Required | Folder name that reflects the installed FactoryTalk Optix Studio
version. |
project_to_export | Required | Path to the OPTIX file of the project to
deploy. |
--location= location | Required | Path to the location where you want to save the FactoryTalk Optix Application . |
--silent | Optional | Make the command output non-verbose in the command prompt. |
--help
Use the
--help
or -h
parameter to
display a summary of the available commands in the command prompt.
TIP:
Using unexpected parameters also displays
help.
"C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio"
--help--version
Use the
--version
parameter to display the FactoryTalk Optix Studio
version."C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio"
--versionProvide Feedback