Variables
A variable is an element that represents a figure or a characteristic of an object
and specifies the value of that characteristic.
Overview
Each variable:
- Contains a DataType attribute
- Can be structured to contain other variables
- Contains descriptive attributes
- Cannot contain objects
TIP:
You cannot remove properties from predefined objects. For example, you cannot remove the
Text
property from a Label
object.Variable values
You can set the value of a variable by specifying:
- A fixed value
- An inherited value from the variable type or object type definition
- A dynamic link that sets the value of a variable based on the value of another variableTIP: To use and display values from a field device or a controller, you must import the tags and variables into the project and synchronize them. Variables imported from a field device or controller are tagged with the communication protocol type used to transfer the value. For more information, see Communication drivers.
Variable examples
For example, a variable can represent:
- The speed of a physical object
- TheSpeedvariable with a numeric (Int32) value defines the speed of the Motor object.

- A style characteristic of a graphic object
- TheText colorvariable defines the color of the Label object.

- Various object properties
- A dynamic link to theEmbeddedDatabase1object defines the Store variable value.

Provide Feedback