Install NuGet packages in Visual Studio Code
Install NuGet packages by using the NuGet Gallery extension.
IMPORTANT:
Rockwell Automation
is not responsible for any third-party software, including but not limited to its
performance, security, updates, or compatibility with our products. Any use of third-party
software is at your own risk, and we do not provide support, warranties, or guarantees for
such software. Users should refer to the respective third-party providers for assistance and
licensing terms.Prerequisites
Set Visual Studio Code as the default external code editor. See Set the default code editor.
- To install NuGet packages in Visual Studio Code
- From the main toolbar, select
Open .NET Solution.The default external code editor opens.TIP: Rockwell Automation recommends usingVisual Studio®2022 orVisual Studio Codeas the default code editor. Some development assistance features may not be available when using a different code editor. - In Visual Studio Code, install the NuGet Gallery extension NuGet Gallery - Visual Studio Marketplace.
- In NuGet Gallery, install the necessary NuGet packages.
- Save theCSPROJfile.
- Compile the project.
Provide Feedback