Pull preview
Pull changes from the remote repository to see conflicts between the local project
and the remote project.
Pull preview interface

Item | Description |
|---|---|
![]() | Rows of highlighted conflicts or changes. |
![]() | Select Take all local to accept all of the local
changes. Select Take all remote to accept all of the changes
in the remote repository. |
![]() | Filter the changes in the preview by displaying All
project content, only Updates to the project, or only
Conflicts in the project. |
![]() | Select |
![]() | Select a conflict to the left in a row to accept the local change. Local history |
![]() | Select a conflict to the right in a row to accept the remote change. Remote history |
![]() | An icon in a row indicates:
|
change
preview
conflict
Provide Feedback