Application variables
Bind the property of a graphic object to a predefined
Application
variable to configure the FTOptixApplication
. For example, bind to the visibility of a property to make the object blink based on a machine or process state.To bind to a variable, see Create dynamic links.The
Application
category in the Dynamic Link browser displays the variables related to the FTOptixApplication
.Variable | Type | Definition | Read or Write | Reboot Required |
|---|---|---|---|---|
Blink fast | Boolean | Variable value that alternates between set for 1 second and cleared for 0.5 seconds. | Read-only | Reboot not required |
Blink medium | Boolean | Variable value that alternates between set for 2 seconds and cleared for 1 second. | Read-only | Reboot not required |
Blink slow | Boolean | Variable value that alternates between set for 3 seconds and cleared for 1.5 seconds. | Read-only | Reboot not required |
application variable
blink fast
blink medium
blink slow
blink
Provide Feedback