Push Agent configuration for the Azure IoT Hub
An example of Push Agent configuration for sending and receiving data with Azure IoT Hub broker.
Property | Value |
|---|---|
ClientId | MyDevice01 |
BrokerIPAddress | contoso.azure-devices.net |
BrokerPort | 8883 |
BrokerTopic | devices/MyDevice01/messages/events/ |
QoS | 1 Azure Iot Hub does not support level 2 QoS. If you use the level 2 QoS, Azure Iot Hub closes the connection every time a message is sent. |
UseSSL | True |
CACert | |
ClientCert | |
ClientCertPassword | |
Username | contoso.azure-devices.net/MyDevice01/?api-version=2018-06-30 |
Password | SharedAccessSignature sig= signature-string &se=expiry &sr=URL-encoded-resourceURI |
Provide Feedback