Communication drivers overview
Some communication drivers may have specific characteristics.
Communication driver | Online tags import | Offline tags import | Custom data types import |
|---|
*
Only for selected controller series. For more information, see S7TCP driver.**
Only for importing tags in the offline mode.
TIP:
You can communicate with controllers that support custom protocols through the serial interface by using the
Serial port
communication driver. For advanced implementations, you can use dedicated C# APIs. See C# API reference.Provide Feedback